FB#.SCALED.DIR
Description
FB#.SCALED.DIR sets the direction of the scaled feedback FB#.SCALED.P relative to the position feedback FB#.P.
| Value | Description |
|---|---|
| 0 | Non-reversing |
| 1 | Reversing |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-07-02-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0,1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
|
| Stored in Non-Volatile Memory | Yes |
Variants Supported
All variants are supported.